MCF51JM128 Bootloader AN3748

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MCF51JM128 Bootloader AN3748

3,483件の閲覧回数
lucas_loizaga
Contributor I

Hi!

Over 5 years ago FSL support sent me the source code of the application of PC AN3748.
Currently I need to run this AN using Windows 64 bits.
The package was updated with AN3748 compatible drivers, but these drivers do not work with the original PC application.
Please could someone from NXP or FSL post the updated source code of the PC application?

Thank you very much,

 

Lucas

ラベル(1)
0 件の賞賛
返信
3 返答(返信)

3,231件の閲覧回数
dariobalina
Contributor I

Hi,

Anyone have backuped the zip containig the AN3748 source code?

There are no traces of it on the web, It seems that many of Freescale's old application notes resources have been removed.

Thank you very much,

Dario

0 件の賞賛
返信

3,231件の閲覧回数
lucas_loizaga
Contributor I

Hello!, anybody here?

0 件の賞賛
返信

3,229件の閲覧回数
vicentegomez
NXP TechSupport
NXP TechSupport

Hi Lucas 

Please check the attached file, this is the last version that I have, 

I hope this will help you.

Regards

Vicente Gomez

0 件の賞賛
返信