M5282LITE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

M5282LITE

1,143 Views
de
Contributor I

Hey guys, I apologize if this is the wrong place for this. I recently was given a M5282LITE development board and I have a couple of questions.

 

1. I notice there are no pin headers on the board. I assume the reason for that is so that the user can solder their wires directly to the board. I will be using this board for hobby purposes only so I would like to solder some pin headers to it. What would be the best kind of solder to use for this board? I haven't done much soldering to PCBs so this is kind of new to me.

 

2. The package that the board came in, says the software on the support CD is for windows 95/98/2000/NT/XP. All of my computers are running Windows 7 on them. Is there any other software that I can use (codewarrior?) for this board? If there is nothing else I can always dual boot my computer with XP.

 

Any help will be greatly appreciated. Thanks!

Labels (1)
0 Kudos
Reply
1 Reply

1,062 Views
Wlodek_D_
Senior Contributor II

Hello,

Thank you for your post, however please consider moving it to the right community place (e.gColdFire/68K Microcontrollers and Processors ) to get it visible for active members.

For details please see general advice Where to post a Discussion?

Thank you for using Freescale Community. 

0 Kudos
Reply