M52277EVB dBug

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

M52277EVB dBug

2,033件の閲覧回数
ianlovatt
Contributor III

Does anyone know why the M52277EVB dBug project available here does not run from flash?

 

http://www.freescale.com/webapp/sps/download/license.jsp?colCode=M52277EVB_DBUG_SRC&location=null&fs... search&Parent_pageType=from search

 

Both RAM and FLASH targets run when debugging in CW but the program fails to start when the EVB is power cycled away from the debugger. Unless I've missed something fundamental about how the dBug project works I believe it should execute from flash like any other program...

 

Cheers

ian

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,576件の閲覧回数
cw_weldon
Contributor I

You can diconnect the Multilink and reset the board to see if this brings it up.

0 件の賞賛
返信

1,576件の閲覧回数
ianlovatt
Contributor III

Yes that's what i'm doing, once the board is flashed it should startup after reset without the multilink connected but it doesn't. I know the h/w is fine as other projects startup ok.

0 件の賞賛
返信