M52259DEMOKIT Does not run standalone, needs debugger to start running

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

M52259DEMOKIT Does not run standalone, needs debugger to start running

跳至解决方案
2,752 次查看
carloscuevas
Contributor III
Hello, I 'm looking forward to use this very nice and cheap DemoKit in a school proyect, but theres something that realy annoys me: I flash the app and run it very nice, I can debug and even I can press reset and close the debugger, the app still runs. But in a power switching (power off and then on) it stops running and I need to run the debugger again and click on "run" to make the app run again. Is there any way to solve this problem? I will really need this board to run standalone. Any help would be very appreciated.
标签 (1)
0 项奖励
回复
1 解答
1,886 次查看
carloscuevas
Contributor III
Thankls a lot for your fast response, but I have found the problem. It seems that using the default firmware on the USBDM was the problem, I upgraded to the new USBDM firmware and also upgraded to CW for CF patch 7.1.2 and the problem is now resolved. I think it was the USBDM that did not let the chip run with the original firmware. Thanks to all.

在原帖中查看解决方案

0 项奖励
回复
2 回复数
1,887 次查看
carloscuevas
Contributor III
Thankls a lot for your fast response, but I have found the problem. It seems that using the default firmware on the USBDM was the problem, I upgraded to the new USBDM firmware and also upgraded to CW for CF patch 7.1.2 and the problem is now resolved. I think it was the USBDM that did not let the chip run with the original firmware. Thanks to all.
0 项奖励
回复
1,886 次查看
mjbcswitzerland
Specialist V

Hi

 

Are you sure that you have really flashed the application?

1) Check that the project's target is set for a FLASH version and not RAM version.

2) Ensure that you have used the FLASH tool to program the generated ELF or SREC.

See the following Kirin3 tutorial for step-by-step guide (see chapter 5):

http://www.utasker.com/docs/M5223X/uTaskerV1-4_M5225X.PDF

 

Regards

 

Mark

 

www.uTasker.com
- OS, TCP/IP stack, USB, device drivers and simulator for M521X, M521XX, M5221X, M5222X, M5223X, M5225X. One package does them all - "Embedding it better..."

 

 

0 项奖励
回复