M52259DEMOKIT Does not run standalone, needs debugger to start running

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

M52259DEMOKIT Does not run standalone, needs debugger to start running

ソリューションへジャンプ
3,619件の閲覧回数
carloscuevas
Contributor III
Hello, I 'm looking forward to use this very nice and cheap DemoKit in a school proyect, but theres something that realy annoys me: I flash the app and run it very nice, I can debug and even I can press reset and close the debugger, the app still runs. But in a power switching (power off and then on) it stops running and I need to run the debugger again and click on "run" to make the app run again. Is there any way to solve this problem? I will really need this board to run standalone. Any help would be very appreciated.
ラベル(1)
0 件の賞賛
返信
1 解決策
2,753件の閲覧回数
carloscuevas
Contributor III
Thankls a lot for your fast response, but I have found the problem. It seems that using the default firmware on the USBDM was the problem, I upgraded to the new USBDM firmware and also upgraded to CW for CF patch 7.1.2 and the problem is now resolved. I think it was the USBDM that did not let the chip run with the original firmware. Thanks to all.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,754件の閲覧回数
carloscuevas
Contributor III
Thankls a lot for your fast response, but I have found the problem. It seems that using the default firmware on the USBDM was the problem, I upgraded to the new USBDM firmware and also upgraded to CW for CF patch 7.1.2 and the problem is now resolved. I think it was the USBDM that did not let the chip run with the original firmware. Thanks to all.
0 件の賞賛
返信
2,753件の閲覧回数
mjbcswitzerland
Specialist V

Hi

 

Are you sure that you have really flashed the application?

1) Check that the project's target is set for a FLASH version and not RAM version.

2) Ensure that you have used the FLASH tool to program the generated ELF or SREC.

See the following Kirin3 tutorial for step-by-step guide (see chapter 5):

http://www.utasker.com/docs/M5223X/uTaskerV1-4_M5225X.PDF

 

Regards

 

Mark

 

www.uTasker.com
- OS, TCP/IP stack, USB, device drivers and simulator for M521X, M521XX, M5221X, M5222X, M5223X, M5225X. One package does them all - "Embedding it better..."

 

 

0 件の賞賛
返信