Linux on MCF5329

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Linux on MCF5329

跳至解决方案
3,884 次查看
srinivasw
Contributor I

Hi,

We have a hardware with MCF5329.   I understnad that this processor is without MMU.

Considering this, is it possible to run latest linux latest linux (may be 4.4.x) on this processor?

OR

What is the latest version of Linux that we can run on MCF5329?

Regards

Srinivasa

标记 (1)
0 项奖励
回复
1 解答
3,831 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I could only confirm there with no official released LTIB(BSP) software package based on Linux Kernel 5.15.4.

You could have a try to check if that works or not.

Best regards,

Mike

 

在原帖中查看解决方案

3 回复数
3,876 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I could find available uCLinux for MCF5329 is quite old (released at 2008): 

Linux-2.6.26-uc0 kernel

Please visit here, customer could download related LTIB BSP and updated patch.

ISO file: 2008 Linux BSP for Freescale M5329EVB Update (07-Jul-2008)

2008 Linux BSP for Freescale M5329EVB Update (07-Jul-2008)

best regards,

Mike

3,839 次查看
srinivasw
Contributor I

Hi Mike,

Thanks for quick reply.

There are some source code in Linux Kernel 5.15.4 related to m53xx as shown in below link:

https://git.kernel.org/pub/scm/linux/kernel/git/stable/linux.git/tree/arch/m68k/coldfire/m53xx.c?id=...

Does it mean that we can use Linux Kernel 5.15.4 for MCF5329?

Please let us know your thoughts.

Regards

Srinivasa

0 项奖励
回复
3,832 次查看
Hui_Ma
NXP TechSupport
NXP TechSupport

Hi,

I could only confirm there with no official released LTIB(BSP) software package based on Linux Kernel 5.15.4.

You could have a try to check if that works or not.

Best regards,

Mike