JM128 Bootloader driver don't work with win7

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

JM128 Bootloader driver don't work with win7

ソリューションへジャンプ
1,803件の閲覧回数
flaviocerato
Contributor I

Hi at all,

I have a problem with the driver of JM128 Bootloader driver.

It work on Windows XP correctly, but i can't install the driver on a Pc with

Windows 7.

When i try to install it i hqve an error because the driver is not correct for

the OS win7.

 

Any can Help me ?

 

Thanks very musch

ラベル(1)
0 件の賞賛
返信
1 解決策
1,467件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

There is available an updated version of JM128 Bootloader GUI compatible with 64-bit operating systems. Please install this version for Win 7.

Good Luck!

Best Regards,

Fang

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,468件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

There is available an updated version of JM128 Bootloader GUI compatible with 64-bit operating systems. Please install this version for Win 7.

Good Luck!

Best Regards,

Fang

0 件の賞賛
返信