Interfacing 8-bit parallel memory with MC9S12XEP100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interfacing 8-bit parallel memory with MC9S12XEP100

2,185 Views
shraddhanagle
Contributor II

Hello,

I have interfaced MC9S12XEP100 with 8-bit (16 address lines) parallel EEPROM where the A0 line of MC9S12XEP100 is connected to A0 line of EEPROM, A1 line of MC9S12XEP100 is connected to A1 line of EEPROM and so on till A15. While accessing the memory HDBE bit in EBICTL0 register is set to zero which implies DATA[15:8], UDS, and LDS disabled and ASIZ is set to 16. However, it is observed that only odd addresses of memory is accessed by the MC9S12XEP100. The A0 line of controller remains at logic HIGH level. 

Is there any way to access the whole 8-bit memory using MC9S12XEP100 for above mentioned hardware configuration?

0 Kudos
Reply
3 Replies

1,988 Views
yibbidy
Contributor V

Hi,

The microprocessor that you are using is not a Coldfire/68K, so you might be better asking your question in the forum for the S12 series:

S12 / MagniV Micro controllers

Cheers,

Shaun

0 Kudos
Reply

1,988 Views
shraddhanagle
Contributor II

Thank you Shaun!

0 Kudos
Reply

1,988 Views
TomE
Specialist II

One of the Admins should be able to move this thread there.


Actually, as the Author, I think there's an option somewhere that lets you move the thread to somewhere else.

Tom

0 Kudos
Reply