I'm using the demo board m52233demo and also I use the interniche coldfire lite TCP/IP stack v3.0
I would like to make a I²C bus to control a LCD graph 128x64, de LCD CONTROLLER is a
STE2002 :http://www.dcdi-video.com/stonline/products/literature/ds/9044.pdf
this has to work on a TCP client. The client is no problem this works very good. But I²C is the big problem.
I found a document "implementing an LCD module to the MCF5223x" (document nuber AN3559).
but I can not get this code to work.
Now is my question: Can someone send me a working code for I²C and maybe also a character set for the LCD controlle.
thanks
已解决! 转到解答。
I can't help you with the I2C stuff, but I do have C code available for a character generator, see attachment.
Bytes in the code are vertically oriented in the characters. Each character consists of 5 bytes. The lowest bit of the first byte is the upper left pixel in the character.
The first character in the character generator corresponds with ASCII code 32 (0x20) .
I can't help you with the I2C stuff, but I do have C code available for a character generator, see attachment.
Bytes in the code are vertically oriented in the characters. Each character consists of 5 bytes. The lowest bit of the first byte is the upper left pixel in the character.
The first character in the character generator corresponds with ASCII code 32 (0x20) .