How much storage with MCF52259 using USB?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How much storage with MCF52259 using USB?

跳至解决方案
3,352 次查看
d_vara
Contributor III

I am proving MC52259EVB board.

Can anyone soy me what is the maximum size of PEN-USB that I can use.

 

I want to save a lot of registers for months. I read that chis uC only can use 1 or 2 Mbytes of external memomry. I am thinking to use a USB to store this information.

I need to know what is the maximum size.

 

thanks.

标签 (1)
0 项奖励
回复
1 解答
2,339 次查看
admin
Specialist II

I'm not sure what kind of limitation you think there is.

1 or 2 Mbytes might refer to the number of address lines of the mini-flexbus interface. It has nothing to do with USB.

2 Gbytes might refer to some kind of limitation of the FAT filesystem. Again, it's not about USB itself. You can choose any filesystem, or work with none at all. That's a design choice, it's yours to make.

There is no fundamental limitation of the maximum size of a USB flash drive. It should be possible to use all of it.

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,339 次查看
d_vara
Contributor III

I read,that anyone use up to 2Gb.

Is it correct?

0 项奖励
回复
2,340 次查看
admin
Specialist II

I'm not sure what kind of limitation you think there is.

1 or 2 Mbytes might refer to the number of address lines of the mini-flexbus interface. It has nothing to do with USB.

2 Gbytes might refer to some kind of limitation of the FAT filesystem. Again, it's not about USB itself. You can choose any filesystem, or work with none at all. That's a design choice, it's yours to make.

There is no fundamental limitation of the maximum size of a USB flash drive. It should be possible to use all of it.

0 项奖励
回复
2,339 次查看
d_vara
Contributor III

Ok, thank you.

I will use USB to storage datas.

Very thanks.

0 项奖励
回复