How much storage with MCF52259 using USB?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How much storage with MCF52259 using USB?

Jump to solution
3,471 Views
d_vara
Contributor III

I am proving MC52259EVB board.

Can anyone soy me what is the maximum size of PEN-USB that I can use.

 

I want to save a lot of registers for months. I read that chis uC only can use 1 or 2 Mbytes of external memomry. I am thinking to use a USB to store this information.

I need to know what is the maximum size.

 

thanks.

Labels (1)
0 Kudos
Reply
1 Solution
2,458 Views
admin
Specialist II

I'm not sure what kind of limitation you think there is.

1 or 2 Mbytes might refer to the number of address lines of the mini-flexbus interface. It has nothing to do with USB.

2 Gbytes might refer to some kind of limitation of the FAT filesystem. Again, it's not about USB itself. You can choose any filesystem, or work with none at all. That's a design choice, it's yours to make.

There is no fundamental limitation of the maximum size of a USB flash drive. It should be possible to use all of it.

View solution in original post

0 Kudos
Reply
3 Replies
2,458 Views
d_vara
Contributor III

I read,that anyone use up to 2Gb.

Is it correct?

0 Kudos
Reply
2,459 Views
admin
Specialist II

I'm not sure what kind of limitation you think there is.

1 or 2 Mbytes might refer to the number of address lines of the mini-flexbus interface. It has nothing to do with USB.

2 Gbytes might refer to some kind of limitation of the FAT filesystem. Again, it's not about USB itself. You can choose any filesystem, or work with none at all. That's a design choice, it's yours to make.

There is no fundamental limitation of the maximum size of a USB flash drive. It should be possible to use all of it.

0 Kudos
Reply
2,458 Views
d_vara
Contributor III

Ok, thank you.

I will use USB to storage datas.

Very thanks.

0 Kudos
Reply