How do I program the MCF51JF128 Flash?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How do I program the MCF51JF128 Flash?

1,163件の閲覧回数
chicagomike
Contributor III

I have a TWR-MCF51JF tower system module and CW v10.1 with the MCF51Jx service pack. I've worked through the quick start lab, and I can build a project and run it on the target using debug mode through USB and the PE terminal tool. My next step is to program the processor flash using the Multilink Universal tool and the BKGD i/f on the processor. Can anyone point me to an example project or a tutorial that walks through this?

 

Thanks,

 

Mike

ラベル(1)
0 件の賞賛
返信
1 返信

1,030件の閲覧回数
ZhangJennie
NXP TechSupport
NXP TechSupport

see below how to set debug configuration to debug code.

debug connection.JPG

0 件の賞賛
返信