How do I program the MCF51JF128 Flash?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I program the MCF51JF128 Flash?

1,204 Views
chicagomike
Contributor III

I have a TWR-MCF51JF tower system module and CW v10.1 with the MCF51Jx service pack. I've worked through the quick start lab, and I can build a project and run it on the target using debug mode through USB and the PE terminal tool. My next step is to program the processor flash using the Multilink Universal tool and the BKGD i/f on the processor. Can anyone point me to an example project or a tutorial that walks through this?

 

Thanks,

 

Mike

Labels (1)
0 Kudos
Reply
1 Reply

1,071 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

see below how to set debug configuration to debug code.

debug connection.JPG

0 Kudos
Reply