GPIO Pin during reset

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

GPIO Pin during reset

跳至解决方案
3,401 次查看
beckm1
Contributor I

Hi all

 

On the project I am working at the moment I am using a MCF5373L processor.

At the beginning the processor stays in reset until a switch desactivate the reset. The switch is connected to the processor (pin FB_CS5, functions of the the switch are used when processor is running) and a CPLD (function of the switch is desactivating of the reset).

 

Found in a thread and also in the Reference Manual, the GPIO are digitial inputs. In the thread is written that a weak pull up is enabled during the reset.

 

(Link: https://community.freescale.com/message/69585#69585)

 

When I press now the button (connected over a PU to 3.3V to GND --> Low active), the signal which is connected to the CF and the CPLD only sinks from 3.3V to arround 3.1V.

 

I tried the same without CPLD (when the button is only connected to the CF) and the result is the same.

 

As it looks like, the GPIO are driven activly high during the reset. But I could not find a proper answer on that neither in the Reference Manual, nor in the Datasheet nor in the forum.

 

Is it like that and are there any possibilitys to change that? As I saw in the posted thread, there is no configuration register for that.

 

Thank you for helping!

标签 (1)
0 项奖励
回复
1 解答
2,965 次查看
TomE
Specialist II

> On the project I am working at the moment I am using a MCF5373L processor.

> At the beginning the processor stays in reset until a switch desactivate the reset.

> The switch is connected to the processor (pin FB_CS5,

>

> Found in a thread and also in the Reference Manual, the GPIO are digitial inputs.

> In the thread is written that a weak pull up is enabled during the reset.

 >

> (Link: CFV2 gpio input pull-up on reset question?)

 

That thread documents the CFV2 chips. You're using a CFV3. There are a lot of differences.

 

Table 2.1 in the manual documents FB_CS5 as having a PRIMARY function of being a Chip Select and being an Output.

 

The reset function of this chip is controlled by:

 

13.3.5.3 Chip Select Pin Assignment Register (PAR_CS)

 

The Reset state of the PAR_CS5 bit (all chip selects, in fact) is for them to be configured as active chip selects.

 

Your hardware designer has connected the switch to a pin that is driven actively high during reset.

 

It won't act like a GPIO until the software has written to PAR_CS to change it.

 

You have to change the hardware to use a different pin (and check all the other pins you're using while you're at it), OR you could add a high value resistor between the pin and the switch so the reset level doesn't interfere with the switch's function during reset. Either way you have to change the hardware.

 

Tom

 

在原帖中查看解决方案

0 项奖励
回复
2 回复数
2,966 次查看
TomE
Specialist II

> On the project I am working at the moment I am using a MCF5373L processor.

> At the beginning the processor stays in reset until a switch desactivate the reset.

> The switch is connected to the processor (pin FB_CS5,

>

> Found in a thread and also in the Reference Manual, the GPIO are digitial inputs.

> In the thread is written that a weak pull up is enabled during the reset.

 >

> (Link: CFV2 gpio input pull-up on reset question?)

 

That thread documents the CFV2 chips. You're using a CFV3. There are a lot of differences.

 

Table 2.1 in the manual documents FB_CS5 as having a PRIMARY function of being a Chip Select and being an Output.

 

The reset function of this chip is controlled by:

 

13.3.5.3 Chip Select Pin Assignment Register (PAR_CS)

 

The Reset state of the PAR_CS5 bit (all chip selects, in fact) is for them to be configured as active chip selects.

 

Your hardware designer has connected the switch to a pin that is driven actively high during reset.

 

It won't act like a GPIO until the software has written to PAR_CS to change it.

 

You have to change the hardware to use a different pin (and check all the other pins you're using while you're at it), OR you could add a high value resistor between the pin and the switch so the reset level doesn't interfere with the switch's function during reset. Either way you have to change the hardware.

 

Tom

 

0 项奖励
回复
2,965 次查看
beckm1
Contributor I

 

> The reset function of this chip is controlled by:

>  

> 13.3.5.3 Chip Select Pin Assignment Register (PAR_CS)

>

> The Reset state of the PAR_CS5 bit (all chip selects, in fact) is for them to be configured as active chip > selects.

> Your hardware designer has connected the switch to a pin that is driven actively high during reset.

>  

> It won't act like a GPIO until the software has written to PAR_CS to change it.

 

 

Hello Tom

 

thank you for your answer.

 

I saw that the primary function of FB_CS5 (and all other chip selects) is being a chip select and that it acts as a output. But I could not see a 100% clearly if it is active driven or high Z.

 

But it actually makes sense this way. I will chose another pin, which acts as GPIO during reset.

 

 

beckm1

0 项奖励
回复