External SRAM interface with 5328

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

External SRAM interface with 5328

2,827 次查看
Soos
Contributor III
I want to interface external 16-bit SRAM & 16-bit FLASH to 5328. I got confused because of split bus mode setting & not sure whether I should connect D0-D15 or D16-D31. I am not using any other type of RAM.
Can anybody help me in this regard ?
Thanks in advance.

标签 (1)
0 项奖励
回复
2 回复数

1,728 次查看
obidon
Contributor III
0 项奖励
回复

1,728 次查看
Soos
Contributor III
Thanks Obidon,
This PDF is realy useful.
- Soos
0 项奖励
回复