External SRAM interface with 5328

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

External SRAM interface with 5328

2,872件の閲覧回数
Soos
Contributor III
I want to interface external 16-bit SRAM & 16-bit FLASH to 5328. I got confused because of split bus mode setting & not sure whether I should connect D0-D15 or D16-D31. I am not using any other type of RAM.
Can anybody help me in this regard ?
Thanks in advance.

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,773件の閲覧回数
obidon
Contributor III
0 件の賞賛
返信

1,773件の閲覧回数
Soos
Contributor III
Thanks Obidon,
This PDF is realy useful.
- Soos
0 件の賞賛
返信