Downlad .s19 file to MCU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Downlad .s19 file to MCU

3,934件の閲覧回数
sebasira
Senior Contributor I

Hello everybody!

 

Is there any software wich I can use to download s19 files to MCU? I mean, I'm using Codewarrior and Hi-Wave for developping and debugging. Now the idea is to give the s19 file to my client so he can download the code to the mcu, using an USB-BDM. I don't want to install Codewarrior and Hi-Wave on his computer... Can I only installa Hi-Wave so he can use it to download the s19 file? Is there any Hi-Wave installer or any other application so he can download the s19 file?

 

Thanks!

ラベル(1)
0 件の賞賛
返信
4 返答(返信)

2,487件の閲覧回数
J2MEJediMaster
Specialist I

Check out the stand-alone software and hardware for flash programming that is offered by P&E Microsystems at www.pemicro.com.

 

---Tom

0 件の賞賛
返信

2,487件の閲覧回数
sebasira
Senior Contributor I

Thanks Tom!

 

I looked into P&E page and I found PROG12Z... Sadly it's not a freeware... So now I'll have to talk to my boss and see if he want to buy it... Is there any other application I can use?

 

 

 

Thanks again!

0 件の賞賛
返信

2,487件の閲覧回数
EdT
Contributor II

Hi Sebastian,

 

Are you working with a ColdFire processor (just a guess since this is in the ColdFire forum)? PROG12Z is the flash programming software for the Freescale HC(S)12(X) processors.

 

For ColdFire devices, the flash programming software is called PROGCFZ. There is a free 64K limited trial version available for you to evaluate:

 

http://www.pemicro.com/downloads/download_file.cfm?download_id=180

 

Best regards,

Edison

0 件の賞賛
返信

2,487件の閲覧回数
sebasira
Senior Contributor I

You're right... I'm at the wrong forum... I'm working with both ColdFire and HCS12....

 

Thanks!

0 件の賞賛
返信