DEMOJM JM128 CDC Terminal Example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

DEMOJM JM128 CDC Terminal Example

4,034 次查看
bryano
Contributor II

The DEMOJM kit comes with the 9S08JM60 and MCF51JM128 modules and CMX USB Lite stack.  We have implemented the JM60 CDC Terminal example into a project.  We now need to move up to the JM128 (as the Flexis line was intended), but there is no CDC terminal example for the JM128 in the DEMOJM kit.   Is there a JM128 CDC terminal example available anywhere?  Has anyone attempted to port it?

 

Thanks.

标签 (1)
0 项奖励
回复
5 回复数

2,688 次查看
David_UCT
Contributor III

Hi

 

I have just checked to be sure, the CMX USB Lite stack comes with a mcf51 cdc demo you can download the mcf51 stack from the website.

 

Regards

 

Dave Wright

0 项奖励
回复

2,688 次查看
bryano
Contributor II

That is a CDC to/from UART example, not a CDC Terminal.  Only the JM60 has the CDC Terminal.  Porting may be the best option.

0 项奖励
回复

2,688 次查看
PG85
Contributor I

I have tried to prt CDC terminal example on JM128 but the issue is with respect to vendor id and product id. Any ideas what values should be used? If I try to use the one in JM60 but it isn't working.

0 项奖励
回复

2,688 次查看
BlackNight
NXP Employee
NXP Employee

Hello,

VID/PID can be the same both for JM60 and JM128.

If you want to use the Freescale USB stack (www.freescale.com/usb) with PHDC (and CDC) support with Processor Expert:

Description and examples are here:

http://mcuoneclipse.wordpress.com/2012/03/15/usb-cdc-reloaded/

 

Erich

0 项奖励
回复

2,688 次查看
gustavod
Contributor III

We have successfully port the CDC terminal example for the MCF51JM128. We used the TWR-LCD kit to test the code. Our project is a open source RTOS. The terminal / USB driver was implemented as a task, but i beleive that you can use the port without the RTOS too.

The link to download the code is:
http://code.google.com/p/brtos/downloads/list

 

The demo project is also attached to this message.

 

Best regards,
Gustavo

 

TWR-LCD.zip

0 项奖励
回复