52257 D4D demo rendering very blurry fonts

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

52257 D4D demo rendering very blurry fonts

1,278 Views
Leong
Contributor III

Finally got the custom board driven by the 52277 working with a 800x480lcd to load and run the demo. The fonts seems to have double edges as in the attachment shown. I tried to change some timing numbers and didn't see any improvement. Any one familiar with the demo or the lcd in general may point me a direction to look at ?

 

Thanks

leong

Labels (1)
0 Kudos
Reply
1 Reply

1,099 Views
TomE
Specialist II

That looks weird. I don't know exactly what it is meant to look like, but I have experience with that LCD controller in the MCF5329. It looks like there's some sort of addressing problem, but I can't imagine how that could happen.

 

Can you code up some really simple graphics test patterns and see how they come out? Simple things like a dingle pixel of saturated colour in a field of black, then try lines. You should also dump the video memory to see if it has the expected content.

 

Are you running 16 bit colour (5-6-5) 18 bits in 32-bit pixels or one of the palette modes?

 

I'd suggest you change the LCD Burst mode to "fixed burst of 20".

 

Also check that you've got the LCDC Crossbar priority higher than the CPU.

 

The following are from MCF5329 code, but the register names should be similar for your one.

 

    MCF_LCDC_LDCR = MCF_LCDC_LDCR_BURST |                    MCF_LCDC_LDCR_HM(0x14) |    /* Burst-copy 20 at */                    MCF_LCDC_LDCR_TM(0x0c);     /* Low water mark 12 */    // Enable bursting from LCD controller to SRAM/SDRAM    MCF_SCM_BCR = 0x3ff;

    MCF_XBS_PRS1 =    MCF_XBS_PRS_M7(0x6) |    /* Factory Test */
                    MCF_XBS_PRS_M6(0x5) |    /* USB OTG */
                    MCF_XBS_PRS_M5(0x4) |    /* USB Host */
                    MCF_XBS_PRS_M4(0x0) |    /* LCD Controller */
                    MCF_XBS_PRS_M2(0x3) |    /* FEC Controller */
                    MCF_XBS_PRS_M1(0x2) |    /* eDMA Controller */
                    MCF_XBS_PRS_M0(0x1);    /* Core */

    MCF_XBS_CRS1 = MCF_XBS_CRS_PARK(0x0);

Tom

 

0 Kudos
Reply