Configuring RAMBAR register

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Configuring RAMBAR register

Jump to solution
2,203 Views
salman83
Contributor II

Hi,

I was reading the documentation for MCF52254. While configuring the RAMBAR register, I do not understand the meaning of bit 5.

 

RAMBAR

 

Address Space Masks

 

C/I = CPU space/interrupt acknowledge cycle mask

 

Also, for FLASHBAR register, is it OK to enable the Address fetch speculation (AFS) bit 6. I have read from other posts that it is creates problem when enabled and it is a bug acknowledged by Freescale.

 

Any help will be highly appreciated.

 

Regards.

Labels (1)
0 Kudos
Reply
1 Solution
2,087 Views
TomE
Specialist II

> I do not understand the meaning of bit 5.

You really need to have followed every Freescale/Motorola part from the 68000 on to understand what the "Address Spaces" mean and what they're used for.

You don't need to know.

The manual says:

Table 12-2. RAMBAR Field Descriptions (continued)

5–1  C/I, SC, SD, UC, UD

    These bits are useful for power management as detailed in Section

     12.3.2, “Power Management.” In most applications, the C/I bit is set


You can believe the above advice. You don't want the SRAM responding to interrupt cycles!


> Also, for FLASHBAR register, is it OK to enable the Address fetch speculation


The Chip Errata document (MCF52259DE.pdf) doesn't list that as a problem for this chip.

> have read from other posts that it is creates problem when enabled

> and it is a bug acknowledged by Freescale.

I can only find this one which indicates you don't have a problem. What did you find?


https://community.freescale.com/message/50265#50265


    I received confirmation from freescale that the "speculaton bug has been fixed in the MCF5225X".

    This means that the workaround is no longer needed for this chip.


Tom


View solution in original post

0 Kudos
Reply
2 Replies
2,087 Views
Monica
Senior Contributor III

Hello Salman!

Were those hints helpful?

Please keep us posted!

Monica

0 Kudos
Reply
2,088 Views
TomE
Specialist II

> I do not understand the meaning of bit 5.

You really need to have followed every Freescale/Motorola part from the 68000 on to understand what the "Address Spaces" mean and what they're used for.

You don't need to know.

The manual says:

Table 12-2. RAMBAR Field Descriptions (continued)

5–1  C/I, SC, SD, UC, UD

    These bits are useful for power management as detailed in Section

     12.3.2, “Power Management.” In most applications, the C/I bit is set


You can believe the above advice. You don't want the SRAM responding to interrupt cycles!


> Also, for FLASHBAR register, is it OK to enable the Address fetch speculation


The Chip Errata document (MCF52259DE.pdf) doesn't list that as a problem for this chip.

> have read from other posts that it is creates problem when enabled

> and it is a bug acknowledged by Freescale.

I can only find this one which indicates you don't have a problem. What did you find?


https://community.freescale.com/message/50265#50265


    I received confirmation from freescale that the "speculaton bug has been fixed in the MCF5225X".

    This means that the workaround is no longer needed for this chip.


Tom


0 Kudos
Reply