ColdFire MCF52259 also Support DSP command operation?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

ColdFire MCF52259 also Support DSP command operation?

Jump to solution
2,122 Views
fish_yu
Contributor III

Hello,everyone

Recently, I study MCF52259 processor for my project. I also want to design my project by using TI DSP processor. But ColdFire, in fact, provide source codes named MQX RTOS for engineer. I want to know The MCF52259 if it is also support DSP command operation? Just like a ARM9 processor which also run a DSP Command. Does it support??

Labels (1)
0 Kudos
Reply
1 Solution
1,384 Views
admin
Specialist II
The MCF5225x family of MCU's are equipped with the EMAC (Enhanced Multiply-Accumulate Unit.) I am not able to compare the DSP functionality of the Coldfire EMAC with that of DSP-enhanced ARM9, though.

View solution in original post

0 Kudos
Reply
1 Reply
1,385 Views
admin
Specialist II
The MCF5225x family of MCU's are equipped with the EMAC (Enhanced Multiply-Accumulate Unit.) I am not able to compare the DSP functionality of the Coldfire EMAC with that of DSP-enhanced ARM9, though.
0 Kudos
Reply