ColdFire MCF52259 also Support DSP command operation?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

ColdFire MCF52259 also Support DSP command operation?

ソリューションへジャンプ
2,180件の閲覧回数
fish_yu
Contributor III

Hello,everyone

Recently, I study MCF52259 processor for my project. I also want to design my project by using TI DSP processor. But ColdFire, in fact, provide source codes named MQX RTOS for engineer. I want to know The MCF52259 if it is also support DSP command operation? Just like a ARM9 processor which also run a DSP Command. Does it support??

ラベル(1)
0 件の賞賛
返信
1 解決策
1,442件の閲覧回数
admin
Specialist II
The MCF5225x family of MCU's are equipped with the EMAC (Enhanced Multiply-Accumulate Unit.) I am not able to compare the DSP functionality of the Coldfire EMAC with that of DSP-enhanced ARM9, though.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,443件の閲覧回数
admin
Specialist II
The MCF5225x family of MCU's are equipped with the EMAC (Enhanced Multiply-Accumulate Unit.) I am not able to compare the DSP functionality of the Coldfire EMAC with that of DSP-enhanced ARM9, though.
0 件の賞賛
返信