ColdFire MCF52259 also Support DSP command operation?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

ColdFire MCF52259 also Support DSP command operation?

跳至解决方案
2,156 次查看
fish_yu
Contributor III

Hello,everyone

Recently, I study MCF52259 processor for my project. I also want to design my project by using TI DSP processor. But ColdFire, in fact, provide source codes named MQX RTOS for engineer. I want to know The MCF52259 if it is also support DSP command operation? Just like a ARM9 processor which also run a DSP Command. Does it support??

标签 (1)
0 项奖励
回复
1 解答
1,418 次查看
admin
Specialist II
The MCF5225x family of MCU's are equipped with the EMAC (Enhanced Multiply-Accumulate Unit.) I am not able to compare the DSP functionality of the Coldfire EMAC with that of DSP-enhanced ARM9, though.

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,419 次查看
admin
Specialist II
The MCF5225x family of MCU's are equipped with the EMAC (Enhanced Multiply-Accumulate Unit.) I am not able to compare the DSP functionality of the Coldfire EMAC with that of DSP-enhanced ARM9, though.
0 项奖励
回复