Code examples for Badge Board (JM128)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Code examples for Badge Board (JM128)

4,422 Views
pvarela
Contributor II

Hi.

Does anyone know where I could obtain information and code examples for badge board?.

There is not link for www.canyourbadgedothis.com.

Thanks

Labels (1)
5 Replies

3,495 Views
anthony_huereca
NXP Employee
NXP Employee

We're investigating why the website is down. In the meantime you can find schematics and manuals here: http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=JMBADGE

 

I've also attached what I believe is the latest version of code for it. I don't have a badge board handy at the moment to try it out myself, but until the website is back up, you can use the attached code to get started.

 

Thanks for your interest in it!

3,495 Views
Pogo
Contributor III

Hello,

I browser the link you provided and try to find the code example for Badge Board. But I can't find any source code for Badge Board. Could you give me the download link or send the code file to me? Thanks a lot

Regards,

Pogo Lin

0 Kudos
Reply

3,495 Views
Harshal
Contributor I

Does I need to change any linker setting.

i am using it in Codewarirror V6.3

 

 

0 Kudos
Reply

3,495 Views
Harshal
Contributor I

error it got when i am debugging is illegal breakpoint.

illegal bp

 

 

0 Kudos
Reply

3,495 Views
Harshal
Contributor I

Will it work with the Codewarrior V6.3

how to deploy it for the HID Device. and working with Visual Studio and C#.net.

any idea :.

 

 

Regards,

Harshal

0 Kudos
Reply