Cannot get MCF51AC256 into FEE mode

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Cannot get MCF51AC256 into FEE mode

跳至解决方案
3,578 次查看
Kaare
Contributor III

Hi,

 

I have a hardware design where we use an external 32.768KHz crystal oscillator. The output looks like this, measured on the XTAL pin:

 

32.768KHz external clock

 

 

The problem is that i cannot get the MCU to switch over to FEE mode! It keeps waiting for MCGSC_OSCINIT, which will never set. Here's the code for clock init:

 

 

void initClock()
{
 // BDIV = 0, HGO = 1, EREFS = Oscillator selected
 MCGC2 = 0x14;

 // CLKS = FLL mode, IREFS = External ref. clock
 MCGC1 = 0x00;

 // Wait until external oscillator has initialized
 while(!MCGSC_OSCINIT) { };

 // DMX32 = 1, DRS = 1 => 39.85MHz CPU clock
 MCGC4 = 0x21;

 // Wait for FLL to acquire new lock
 while(!MCGSC_LOCK) { };
}

 

 

If i don't call the initClock, then my program will run jsut fine on the internal clock. Adding this routine makes the program stop at MCGSC_OSCINIT, waiting for it to be set, but this never happens!

 

What am i doing wrong here?

 

Regards, Kaare Mai

标签 (1)
0 项奖励
回复
1 解答
2,750 次查看
Kaare
Contributor III

I finally found the solution! It never crossed my mind that the COP watchdog would timeout when i was waiting for the oscillator to lock.

 

I also didn't know that i had to write to SOPT and SOPT2 even though i would like to use the default settings. This is documented in the reference manual for MCF51AC section 5-2:

 

"Even if the application uses the default reset settings of COPE, COPCLKS, and COPT, the user must write to the write-once SOPT and SOPT2 registers during reset initialization to lock in the settings."

 

After disabling the COP or making the code in the OSCINIT wait loop reset the COP, i finally got it to switch to FEE mode.

在原帖中查看解决方案

0 项奖励
回复
4 回复数
2,750 次查看
kef
Specialist I

I think you need to set ERCLKEN bit.

 

Try creating new Project and let Device Initialize or Processor Expert initialize MCG for you.

0 项奖励
回复
2,750 次查看
Kaare
Contributor III

I don't think thats the case. According to figure 16-1 MCG block diagram, ERCLKEN only makes the external clock available as MCGERCLK.

 

Alos, i can't get processor expert to set the correct settings for DMX32 and DCO. One of them is just not available as a setting, i don't know why.

0 项奖励
回复
2,750 次查看
Kaare
Contributor III

The device init / processor expert is complete rubbish.

 

I can't set BDIV, DMX32 and DCO.

 

Also, it does not change IREFS to 0 even tho i enable the external clock and set it to crystal.

 

According to the block diagram IREFS has to be 0 to gate the external clock to the FLL circuit.

0 项奖励
回复
2,751 次查看
Kaare
Contributor III

I finally found the solution! It never crossed my mind that the COP watchdog would timeout when i was waiting for the oscillator to lock.

 

I also didn't know that i had to write to SOPT and SOPT2 even though i would like to use the default settings. This is documented in the reference manual for MCF51AC section 5-2:

 

"Even if the application uses the default reset settings of COPE, COPCLKS, and COPT, the user must write to the write-once SOPT and SOPT2 registers during reset initialization to lock in the settings."

 

After disabling the COP or making the code in the OSCINIT wait loop reset the COP, i finally got it to switch to FEE mode.

0 项奖励
回复