CMX OTG on coldfire

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CMX OTG on coldfire

1,644件の閲覧回数
LPs1978
Contributor III

Hi all,

    I'm starting evaluating the CMX USB LITE for ColdFire. I'm a nubble in USB matters...(readers are advised :smileywink:)

 

I'm analyzing the USB OTG demo and something is not so clear.

 

As far as I know the MCF2221 has a USB OTG internal module, but in the example an external I2C to USB OTG converter is used: MAX 3353.

 

In the code you can see that routintes refer to I2C module to communicate with this device to allow to use this type of USB.

 

My first question is: Am I in wrong or doesn't CMX USB LITE  support the internal ColdFire module?

 

I'll start a new application with MCF52252AF80, do someone have ported this stack to an 5225X coldfire?

 

Thank you!!

ラベル(1)
0 件の賞賛
返信
1 返信

925件の閲覧回数
LPs1978
Contributor III

Ok, I understand a little bit better the demo.

The MAX3353 is used to manage the role of OTG.

 

Means this that I cannot perform all with USB OTG module of ColdFire ?

0 件の賞賛
返信