CFFlasher command line problems

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CFFlasher command line problems

4,482 Views
oed
Contributor I
Hello:

I'm trying to used cfflasher.exe from console, for automatizate the process to program my colfire.

But I don't know how to specify the velocity of the USB, when I use the cfflasher in windows change the speed of the usb to 10 or not works.

I have this command, only need how to set de speed:

$ cfflasher -t M52235EVB -p exampe.elf -s -bdm PE_USB_ML

Thanks!
Labels (1)
0 Kudos
Reply
2 Replies

1,809 Views
oed
Contributor I
Or... another flasher program that can execute from command line? in windows.

Thanks!

PD: The idea is automatice the process to flash my mcf5213 in my eclipse IDE.
0 Kudos
Reply

1,809 Views
Nouchi
Senior Contributor II
Hello,

You could use CPROGCFZ from P&E Micro, but it's not a free solution.
There was a linux BDM solution in the past for 68332, maybe you be inspired by this:
http://cmp.felk.cvut.cz/~pisa/



regards,
Emmanuel
0 Kudos
Reply