CAN BUS bootloader for MCF51JM AN4511SW GUI source code

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CAN BUS bootloader for MCF51JM AN4511SW GUI source code

2,671 Views
adrianb
Contributor II


Hello,

 

I'm using the AN4511, i was able to use this bootloader but i didn't find the source code for the windows application, made in visual studio.

It's there anyone who has the source code?

 

http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4511.pdf?fsrch=1&sr=4&pageNum=1

 

Thanks you,

Adrian.

Labels (1)
4 Replies

2,306 Views
adrianb
Contributor II

Hi,

Thank you!

0 Kudos
Reply

2,306 Views
miduo
NXP Employee
NXP Employee

Hi,

Please find below attachment of the GUI source code. Hope it is helpful.

2,306 Views
TomE
Specialist II

Can you get this put up on NXP's pages for this chip? That would make it easier for everyone to find it later.

Tom

0 Kudos
Reply

2,306 Views
miduo
NXP Employee
NXP Employee

Hi, Tom

Sure! I had put a request on this and hope it will been put on the web page soon.

Best Regards,

Fang

0 Kudos
Reply