CAN BUS bootloader for MCF51JM AN4511SW GUI source code

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN BUS bootloader for MCF51JM AN4511SW GUI source code

2,659件の閲覧回数
adrianb
Contributor II


Hello,

 

I'm using the AN4511, i was able to use this bootloader but i didn't find the source code for the windows application, made in visual studio.

It's there anyone who has the source code?

 

http://cache.nxp.com/files/microcontrollers/doc/app_note/AN4511.pdf?fsrch=1&sr=4&pageNum=1

 

Thanks you,

Adrian.

ラベル(1)
4 返答(返信)

2,294件の閲覧回数
adrianb
Contributor II

Hi,

Thank you!

0 件の賞賛
返信

2,294件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi,

Please find below attachment of the GUI source code. Hope it is helpful.

2,294件の閲覧回数
TomE
Specialist II

Can you get this put up on NXP's pages for this chip? That would make it easier for everyone to find it later.

Tom

0 件の賞賛
返信

2,294件の閲覧回数
miduo
NXP Employee
NXP Employee

Hi, Tom

Sure! I had put a request on this and hope it will been put on the web page soon.

Best Regards,

Fang

0 件の賞賛
返信