Bootloader USB MSD on MCF52254

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bootloader USB MSD on MCF52254

1,818 Views
neXXtep
Contributor I

Hi !

 

I am trying to use the Bootloader USB MSD v3_2 (USB Bootloader V2 Blinks LED1 project) on a custom board with a MCF52254.

I just changed three things :

- the LED pin (Port TC0 to Port TC2)

- the button or jumper pin (Port NQ5 to Port AN5)

- remove debug (no debug on MCF52254, Port DD doesn't exist) 

 

I have the following problem :

If I use my debbuger (AxBDM CF -> a TLBCF : http://www.axman.com/node/303), everything works good !

If I program the MCF52254, nothing happens !

 

I am sure that it is a problem with the .lcf file.

I think when I program, the reset vector is false 

 

If somebody can help me...

Thanks by advance !

 

Thomas 

Labels (1)
0 Kudos
Reply
1 Reply

1,130 Views
davpag
Contributor I

I have the same problem with MCF52255!

0 Kudos
Reply