BDM debugger lost connection to M52223EVB MCU

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BDM debugger lost connection to M52223EVB MCU

ソリューションへジャンプ
4,182件の閲覧回数
DaStoned
Contributor II
Hi

I am using a M52223EVB board together with P&E Micro's USB ColdFire Multilink debugger. Last week I flashed the onboard ColdFire MCU with some new code (using CF Flasher 3.1) and after that it stopped responding. The debugger reports that it cannot force the MCU into background mode. I am assuming that this freeze is caused by my hardware initialization code.

How could I undo the damage? Can I somehow clear the Flash inside the MCU? Can I convince the debugger to communicate with the MCU?

Some details:

The MCU internal clock is running at 48 MHz (checked CLKOUT with oscilloscope), reset works (the RESET led blinks when debugger tries to connect) and the debugger works OK with a "good" M52223EVB board. Also tried a second Multilink debugger, no good. Power, USB and BDM connections are OK.

I have - unfortunately - replicated the exact same situation on a product board (containing the same ColdFire 52223 MCU). Hence the assumption that the problem is caused by software.

The code in question is attached.

The error message from CFFlasher is: "Could not force processor into background mode. Check your connections, power, and specified parallel port."

The error message from P&E PROGCFZ programmer is "Can't communicate with the target processor! Please check your connections between the cable and make sure the target has power"

All suggestions are kindly welcome.
ラベル(1)
0 件の賞賛
返信
1 解決策
2,560件の閲覧回数
DaStoned
Contributor II
It seems I accidentally secured the flash. Using the P&E Micro Unsecure_CF utility, I restored the board to working condition.

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
2,561件の閲覧回数
DaStoned
Contributor II
It seems I accidentally secured the flash. Using the P&E Micro Unsecure_CF utility, I restored the board to working condition.
0 件の賞賛
返信
2,560件の閲覧回数
Wesley
Contributor I
Dear DaStoned,
Nice to meet you. I am a student.I secured the flash. Using the P&E Micro Unsecure_CF utility, I want to restored the board to working condition.But I can't download Unsecure_CF in https://www.pemicro.com/.
Could you send this utility to my [email protected].
Thank you.
I need your help.
                                                                                                                                                Wesley
                                                                                                                                            2008-12-29
0 件の賞賛
返信
2,560件の閲覧回数
DaStoned
Contributor II
The Unsecure CF utility is available on the following address:
https://www.pemicro.com/login.cfm?from_url=/downloads/download_file.cfm?download_id=228

Before downloading it, however, you must register an account on the P&E web page.

Message Edited by DaStoned on 2008-12-29 04:12 PM
0 件の賞賛
返信