Assembly Style Coding

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Assembly Style Coding

2,191件の閲覧回数
carlosmscabral
Contributor I
Hello there,

I use the MCF52221 in a MCF52221DEMO evb.
I would like to know if there is a way to write a code ONLY in assembly ( a simple program, didatic purpose only) WITHOUT using C. That is, I want to edit a code mycode.s (mycode.asm), and use the assembler directly, without compilation. I couldn't find such an option in CodeWarrior.

Thanks,

Carlos Cabral
ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,362件の閲覧回数
carlosmscabral
Contributor I
Thanks...everything I needed!
0 件の賞賛
返信

1,362件の閲覧回数
CompilerGuru
NXP Employee
NXP Employee
This thread

http://forums.freescale.com/freescale/board/message?board.id=CWCFCOMM&message.id=968

is about an assembly only project for a MCF52230.

Daniel
0 件の賞賛
返信