Assembly Style Coding

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Assembly Style Coding

2,303 Views
carlosmscabral
Contributor I
Hello there,

I use the MCF52221 in a MCF52221DEMO evb.
I would like to know if there is a way to write a code ONLY in assembly ( a simple program, didatic purpose only) WITHOUT using C. That is, I want to edit a code mycode.s (mycode.asm), and use the assembler directly, without compilation. I couldn't find such an option in CodeWarrior.

Thanks,

Carlos Cabral
Labels (1)
0 Kudos
Reply
2 Replies

1,474 Views
carlosmscabral
Contributor I
Thanks...everything I needed!
0 Kudos
Reply

1,474 Views
CompilerGuru
NXP Employee
NXP Employee
This thread

http://forums.freescale.com/freescale/board/message?board.id=CWCFCOMM&message.id=968

is about an assembly only project for a MCF52230.

Daniel
0 Kudos
Reply