Any higher processor supports HTTP authentication then MCF5223X series?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Any higher processor supports HTTP authentication then MCF5223X series?

1,348件の閲覧回数
TVNAIDU
Contributor III

Any higher processor supports HTTP authentication then MCF5223X series?. Like password auth, also change passwords, different user accounts like it comes in Embedded LINUX tiny web server. Looking in micro-controller like MCF5223x series only,

ラベル(1)
0 件の賞賛
返信
1 返信

1,037件の閲覧回数
scifi
Senior Contributor I

I'm not sure I understood the question.

Anyway, I have implemented a web server with HTTP Digest Authentication on a MCF5223x. HTTP Basic Authentication would be even easier to implement. User accounts would be trivial to do as well. So yes, it is possible.

0 件の賞賛
返信