Any higher processor supports HTTP authentication then MCF5223X series?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Any higher processor supports HTTP authentication then MCF5223X series?

1,381 Views
TVNAIDU
Contributor III

Any higher processor supports HTTP authentication then MCF5223X series?. Like password auth, also change passwords, different user accounts like it comes in Embedded LINUX tiny web server. Looking in micro-controller like MCF5223x series only,

Labels (1)
0 Kudos
Reply
1 Reply

1,070 Views
scifi
Senior Contributor I

I'm not sure I understood the question.

Anyway, I have implemented a web server with HTTP Digest Authentication on a MCF5223x. HTTP Basic Authentication would be even easier to implement. User accounts would be trivial to do as well. So yes, it is possible.

0 Kudos
Reply