ADC trigger with FTM1 module

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

ADC trigger with FTM1 module

984 次查看
Florijan
Contributor III

Hello, 
I have the application in which I have to control the proportional valve with PWM signal. I have an analog voltage feedback from this valve about how much current flows through this valve. So my idea is to generate a PWM signal with FTM1 module and measure voltage with ADC. So my question is how can I set up the FTM1 and ADC to make a voltage measurement while PWM signal is on logic "1" not "0". Is this possible to use FTM1 
module to do both at the same time (generating PWM signal and generating a hardware trigger for ADC)? If yes, how? 
Best regard, 
Florijan

标签 (1)
0 项奖励
回复
1 回复

776 次查看
TomE
Specialist II

What's the PWM rate? If it is slow enough (relative to the CPU execution speed) then have the PWM also trigger and interrupt and read it during the interrupt.

 

If the interrupt isn't at a convenient time, start TWO timers, one for the PWM and the other one for the interrupt. If the PWM is constant frequency they should stay in sync.

 

If the PWM is too fast, then just have the ADC sample all the time, and pick the right ones in software (the maximum, minimum, ones at the end of the on-slope or whatever).

 

Or add peak-hold hardware and just read the peak voltage if the control loop can handle the filter.

 

Tom

 

0 项奖励
回复