512K in V2 single chips?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

512K in V2 single chips?

4,354件の閲覧回数
Ricardo_RauppV
Contributor I
 
Hi poople

We have a 200K design running in a single chips 5213.We need to implement new features wich will not fit into 256K.What is the next Freescale solution for this design?We have a strong cost competition problem.At a glance a V2 512K single chip would be the very best for it.I took a look into external memory devices, but the cost envolved in power and memories arrangement are too high for this design.The design is entirely based on CodeWarrior 6.4, wich we would like to keep.
Thanks
Ricardo Raupp

 
ラベル(1)
0 件の賞賛
返信
5 返答(返信)

2,424件の閲覧回数
macl
Senior Contributor I
Hi Ricardo,
  Freescale also offers the MCF5216 which is very similar to the 5213.  It has 512K flash.  Also, there is the 5282 which has an 80Mhz option plus an Ethernet controller.
 
FeaturesMCF5213MCF5216
Freq. (MHz)66, 8066
MIPS (Dhrystine 2.1)7663
Flash (KB)256512
SRAM (KB)3264
Memory Controller-SDR SDRAM
CAN11
 
Here is a link to the MCF521X website for more details. 
0 件の賞賛
返信

2,424件の閲覧回数
Ricardo_RauppV
Contributor I
Marc
I took a loot at 5216 /5282 specs and price.
In fact it is a nice solution, but the SDRAM controller,250 pins BGA pack, etc seems to make it a not cost effective solution as a pure 5213 (single chip) with 512K of memory.
The price increase too much when entering in this kind of "not single chips" chips.
Has Freescale a roadmap for devices like 5213 wich comprise bigger memories...?
Thanks !!
0 件の賞賛
返信

2,424件の閲覧回数
macl
Senior Contributor I
Hi Ricardo,
  Yes, Freescale is working on a new ColdFire V2 device with 512k flash that is scheduled to sample to alpha customers in the summer of 2008.
 
Regards,
Mac
0 件の賞賛
返信

2,424件の閲覧回数
Alaric
Contributor I
Hi Mac,

Same problem with running short of code space but on the MCF52233 part.

We are looking for a replacement for the MCF52233 but with 512K Flash so any
draft documentation on this NEW Coldfire V2  so we can compare features would be appreciated.
I heard something about code named "Striker" is this true?

Regards,
Alaric
0 件の賞賛
返信

2,424件の閲覧回数
macl
Senior Contributor I
I'll have to check on that and get back with you.
0 件の賞賛
返信