script executing without CW starting(excuse me for mistake)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

script executing without CW starting(excuse me for mistake)

Jump to solution
1,944 Views
s_kalop
Contributor I

Hello.

I want to load and start program for MSC8156ADS without starting CW. Can i execute *.tcl-script(intended for Debugger Shell originally) in windows command line without CW starting?. Can i use debugger without IDE starting, just by comman line control?

Thank you.

 

Labels (1)
0 Kudos
Reply
1 Solution
1,783 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi Pavel,

I'm afraid that the answer for this case will be short: No, it is not possible.

The StarCore Debugger works only in conjunction with the IDE.

FYI, only the project build can be executed without opening the IDE.

Best regards,

Daniel

View solution in original post

0 Kudos
Reply
1 Reply
1,784 Views
Daniel_Popa
NXP Employee
NXP Employee

Hi Pavel,

I'm afraid that the answer for this case will be short: No, it is not possible.

The StarCore Debugger works only in conjunction with the IDE.

FYI, only the project build can be executed without opening the IDE.

Best regards,

Daniel

0 Kudos
Reply