script executing without CW starting(excuse me for mistake)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

script executing without CW starting(excuse me for mistake)

跳至解决方案
1,349 次查看
s_kalop
Contributor I

Hello.

I want to load and start program for MSC8156ADS without starting CW. Can i execute *.tcl-script(intended for Debugger Shell originally) in windows command line without CW starting?. Can i use debugger without IDE starting, just by comman line control?

Thank you.

 

标签 (1)
0 项奖励
回复
1 解答
1,187 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi Pavel,

I'm afraid that the answer for this case will be short: No, it is not possible.

The StarCore Debugger works only in conjunction with the IDE.

FYI, only the project build can be executed without opening the IDE.

Best regards,

Daniel

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,188 次查看
Daniel_Popa
NXP Employee
NXP Employee

Hi Pavel,

I'm afraid that the answer for this case will be short: No, it is not possible.

The StarCore Debugger works only in conjunction with the IDE.

FYI, only the project build can be executed without opening the IDE.

Best regards,

Daniel

0 项奖励
回复