downloading Codewarrior 10.9 for Linux

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

downloading Codewarrior 10.9 for Linux

ソリューションへジャンプ
3,691件の閲覧回数
d_li
Contributor III

I can't seem to find a codewarrior 10.9 install for linux. The file on the site seems to only have the toolchain and not eclipse. I have not been able to find one w/ eclipse, but the readme from the toolchain archive seems to indicate that it should be used with the eclipse based IDE

ラベル(1)
0 件の賞賛
返信
1 解決策
3,179件の閲覧回数
d_li
Contributor III

Found out there is actually no codewarrior 10.9 IDE for linux. The build chain is there but no eclipse IDE.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,180件の閲覧回数
d_li
Contributor III

Found out there is actually no codewarrior 10.9 IDE for linux. The build chain is there but no eclipse IDE.

0 件の賞賛
返信
3,179件の閲覧回数
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi David,

The CodeWarrior for StarCore 3900 FP is the the only CodeWarrior Software that matches the version 10.9.0 and it can be downloaded from this link

CodeWarrior Dev Tools for StarCore 3900FP DSP|NXP

Regards,

0 件の賞賛
返信