downloading Codewarrior 10.9 for Linux

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

downloading Codewarrior 10.9 for Linux

Jump to solution
3,796 Views
d_li
Contributor III

I can't seem to find a codewarrior 10.9 install for linux. The file on the site seems to only have the toolchain and not eclipse. I have not been able to find one w/ eclipse, but the readme from the toolchain archive seems to indicate that it should be used with the eclipse based IDE

Labels (1)
0 Kudos
Reply
1 Solution
3,284 Views
d_li
Contributor III

Found out there is actually no codewarrior 10.9 IDE for linux. The build chain is there but no eclipse IDE.

View solution in original post

0 Kudos
Reply
2 Replies
3,284 Views
d_li
Contributor III

Found out there is actually no codewarrior 10.9 IDE for linux. The build chain is there but no eclipse IDE.

0 Kudos
Reply
3,284 Views
jorge_plascencia
NXP TechSupport
NXP TechSupport

Hi David,

The CodeWarrior for StarCore 3900 FP is the the only CodeWarrior Software that matches the version 10.9.0 and it can be downloaded from this link

CodeWarrior Dev Tools for StarCore 3900FP DSP|NXP

Regards,

0 Kudos
Reply