bootloader in msc8151

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

bootloader in msc8151

1,556件の閲覧回数
David_usami
Contributor I

Initially, I want to boot MSC8151 from RapidIO mode. In our board, the host external device is a FPGA chip. Here I have a big trouble in RapidIO boot mode because FPGA fail to initialize the RapidIO port.  I doubt that the bootloader in DSP may not run. Up to now, I am not sure if the bootloader is runing.    I have configured RCW as RapidIO boot mode, where RCWLR = 32'h02230000, RCWHR = 32'h01c01e10.  I wonder how I am able to judge if the bootloader in 8151 starts to run when I power on.   Thanks!

ラベル(1)
0 件の賞賛
返信
1 返信

1,378件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Please kindly refer to SR 1-1263920098.

0 件の賞賛
返信