MSC8102ADS and CodeWarrior problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MSC8102ADS and CodeWarrior problem

Jump to solution
3,426 Views
Kiai
Contributor I

Hello,

 

I'm trying to follow the instructions written here

http://www.freescale.com/files/dsp/doc/app_note/AN2460.pdf

about opening a new Stationery Project with CodeWarrior to use on the MSC8102ADS.

 

The problem is:

In instruction "2.1 Create a new CW Project for the MSC8102ADS"

I need to choose at the window with the title bar "New Project"  the option "MSC8102ADS", but it's not there.

There are many other options, but not this specific one.

 

The closest option I see there is MSC8101ADS,

and when I choose that, it gives me an error when I try to Debug: "reset target failed".

 

Is there a way to get this option to appear in the window?

I tried looking for it in this site and Google but I could find the solution...

 

Thank you very much,

Kiai.

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,631 Views
Kiai
Contributor I

Hey,

 

Thank you for the fast reply.

 

I solved the problem:

It seems that you can choose MSC8101ADS from 2 places in that menu.

I chose the MSC8101ADS under SmartDSP and it worked.

I used the last version, downloaded from freescale.com site.

 

 

I'll probably ask something else later =)

Thanks,

Kiai

 

View solution in original post

0 Kudos
Reply
2 Replies
2,631 Views
CrasyCat
Specialist III

Hello

 

- Which version of CodeWarrior are you using?
  To retrieve that info:
  - Start CodeWarrior
  - Select Help -> About Freescale CodeWarrior
  - Click on "Install Products"
  - CodeWarrior version used is displayed on top in the Installed Products dialog.

 

CrasyCat

2,632 Views
Kiai
Contributor I

Hey,

 

Thank you for the fast reply.

 

I solved the problem:

It seems that you can choose MSC8101ADS from 2 places in that menu.

I chose the MSC8101ADS under SmartDSP and it worked.

I used the last version, downloaded from freescale.com site.

 

 

I'll probably ask something else later =)

Thanks,

Kiai

 

0 Kudos
Reply