LINK ERROR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,851件の閲覧回数
ITCO00
Contributor III

Hi,

 

I'm working with CW 10.1.3 for MSC8156 StarCore DSP.

I've received the following link error with no additional interpretation:

 

 

[SCC,2,1027,-1]:ERROR: Non-zero return status from "C:\Program Files\Freescale\CW SC v10.1\eclipse\..\SC\StarCore_Support\compiler\bin\sc3000-ld.exe".
mingw32-make: *** [8156ADS_FILE.eld] Error 1

 

[SCC,2,1027,-1]:ERROR: Non-zero return status from "C:\Program Files\Freescale\CW SC v10.1\eclipse\..\SC\StarCore_Support\compiler\bin\sc3000-ld.exe".mingw32-make: *** [8156ADS_FILE.eld] Error 1

 

What might cause this problem? How can I get more information about the error?

 

Thanks

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
2,036件の閲覧回数
ITCO00
Contributor III

It is a DDR memory overflow problem.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,037件の閲覧回数
ITCO00
Contributor III

It is a DDR memory overflow problem.

0 件の賞賛
返信