LINK ERROR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LINK ERROR

Jump to solution
2,865 Views
ITCO00
Contributor III

Hi,

 

I'm working with CW 10.1.3 for MSC8156 StarCore DSP.

I've received the following link error with no additional interpretation:

 

 

[SCC,2,1027,-1]:ERROR: Non-zero return status from "C:\Program Files\Freescale\CW SC v10.1\eclipse\..\SC\StarCore_Support\compiler\bin\sc3000-ld.exe".
mingw32-make: *** [8156ADS_FILE.eld] Error 1

 

[SCC,2,1027,-1]:ERROR: Non-zero return status from "C:\Program Files\Freescale\CW SC v10.1\eclipse\..\SC\StarCore_Support\compiler\bin\sc3000-ld.exe".mingw32-make: *** [8156ADS_FILE.eld] Error 1

 

What might cause this problem? How can I get more information about the error?

 

Thanks

Labels (1)
Tags (1)
0 Kudos
Reply
1 Solution
2,050 Views
ITCO00
Contributor III

It is a DDR memory overflow problem.

View solution in original post

0 Kudos
Reply
1 Reply
2,051 Views
ITCO00
Contributor III

It is a DDR memory overflow problem.

0 Kudos
Reply