I'm a student. In a project for my Bachelor of Science Degree i have to implement in C a LMS algorithm. The algorithm is put in an IIR noth filter. The error signal for the adaptive filter is e(n)=-y(n). I implemented the algorithm but it doesen't work. I applied a signal at the input of the filter. The signal is a sinusoid limited at half of the amplitude. The filter should increase/decrease it's notch frequency until it matches the frequency of the signal. Instead the notch frequency becomes 0. Here is the C program, it is something wrong in it. I also put the matlab program with which I generate the signal for the C program. I also put a function the matlab program uses.
-----------------------------iir.c-------------------------------------
#include <prototype.h>
#include <stdio.h>
#define DataBlockSize 128 /* the size of a data block */
#define BlockLength 50 /* the number of the data blocks */
Word16 x[DataBlockSize],y[DataBlockSize],e[DataBlockSize];
Word16 w,w1,w2,_miu1=WORD16(0.05),_miu2=WORD16(0.0666),rho=WORD16(0.8),aux,aux2;
//Word16 b[]={WORD16(b0/2), WORD16(b1/2), WORD16(b2/2)};
//Word16 a[]={WORD16(a1/2), WORD16(a2/2)};
Word16 b[]={WORD16(0.5), WORD16(-1.4142/2), WORD16(0.5)};
Word16 a[]={WORD16(-1.1314/2), WORD16(0.64/2)};
Word32 sum;
int main()
{
short n,i;
FILE *fpx,*fpy;
fpx=fopen("x.dat","r+b");
if (!fpx)
printf("\nIt didn't opened");
fpy=fopen("y.dat","w+b");
if (!fpy)
printf("\nIt didn't opened");
for (i=0; i<BlockLength; i++)
{
fread(x,sizeof(Word16),DataBlockSize,fpx);
for (n=0; n<DataBlockSize; n++)
{
sum = L_deposit_h(shr(x[n],1));
sum = L_msu(sum,a[0],w1);
sum = L_msu(sum,a[1],w2);
w = shl(round(sum),1);
sum = L_mult(b[0],w);
sum = L_mac(sum,b[1],w1);
y[n]= shl(mac_r(sum,b[2],w2),1);
w2=w1;
w1=w;
e[n]=-y[n];
if(e[n]<0)
aux=-div_s(-e[n],_miu1);
else
aux=div_s(e[n],_miu1);
if(x[n]<0)
aux2=-div_s(-x[n],_miu2);
else
aux2=div_s(x[n],_miu2);
aux=mult(aux,aux2);
b[1]=add(b[1],aux);
//b[1]=b[1]+miu*e[n]*x[n];
a[0]=mult(rho,b[1]);
//a[0]=rho*b[1];
}
fwrite(y,sizeof(Word16),DataBlockSize,fpy);
}
fclose(fpx);
fclose(fpy);
return(0);
}
---------------------------matlab.m--------------------------------
clear all
close all
clc
Fs = 6400;
w0=2*pi/8;
miu=300;
b=[1 -2*cos(w0) 1]
a=[1 -2*0.8*cos(w0) 0.64]
figure(1),freqz(b,a)
figure(2),zplane(b,a)
% Simulation with a sinusoidal signal with the amplitude limited at half of the sinuoid's
% amplitude
t=0:1/Fs:1-1/Fs; % 1 secs @ 6,4kHz sample rate
W=2*pi*Fs/12;
for i=1:6400
x(i)=min(cos(W*t(i)),0.5);
x(i)=max(x(i),-0.5);
%x(i)=cos(W*t(i));
end
x=0.01*x;
k=fix(length(x)/128);
L=k*128;
fid=fopen('..\x.dat','w','b');
fwrite(fid,x.*2^15,'int16');
fclose(fid);
display('PRESS A KEY');
pause
fid=fopen('..\y.dat','r','b');
y=fread(fid,L,'int16');
fclose(fid);
y=y'/(2^15);
for i=1:L
%adaptive filter
if i<=2
if i==1
[y_ref(i),b,a,e]=filtru_adaptiv_notch([0 0 x(i)],[0 0],a,b,miu);
else
[y_ref(i),b,a,e]=filtru_adaptiv_notch([0 x(i-1:i)],[0 y_ref(i-1)],a,b,miu);
end
else
[y_ref(i),b,a,e]=filtru_adaptiv_notch(x(i-2:i),y_ref(i-2:i-1),a,b,miu);
end
end
n=0:L-1;
w=-pi:2*pi/Fs:pi-2*pi/Fs;
figure(3),plot(w,abs(fftshift(fft(x))));%plot(n,x)
xlabel('Normalized frequencies');
ylabel('Amplitude');
w=-pi:2*pi/512:pi-2*pi/512;
figure(4),plot(w,abs(fftshift(fft(y_ref(6400-512+1:6400)))));
xlabel('Normalized frequencies');
ylabel('Amplitude');
figure(5),plot(w,abs(fftshift(fft(y(6400-512+1:6400)))));%plot(n,y),grid
xlabel('Normalized frequencies');
ylabel('Amplitude');
-----------------------adaptive_notch_filter.m---------------------------
function [y,b,a,e]=adaptive_notch_filter(x,y,a,b,miu)
r=0.8;
y=2*(x(3-0)*b(1+0)/2+(y(3-1)*(-a(1))/2+x(3-1)*b(1+1)/2+x(3-2)*b(1+2)/2+y(3-2)...
*(-a(2))/2))
y=y/4;
e=-y;
b=[b(1) b(1+1)+miu*e*x(3) b(3)];
a=[a(1) r*b(2) a(3)];
已解决! 转到解答。
Hi radustefan,
Does your code solve the nonlinear least-square problem or have you any idea in this sense?
thank you in advance!