Causing Virtual Interrupts from the Debugger?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Causing Virtual Interrupts from the Debugger?

ソリューションへジャンプ
2,206件の閲覧回数
kiliant3072
Contributor I

Hi,

 

I'm wondering whether it is possible to generate a virtual interrupt by writing a value to the appropriate memory location on the 8156. I tried but it only works from inside the program when running on an ADS board and not from the debugger.

 

The goal is to use TCL to stimulate an interrupt i.e. through a change or mem command. This doesn't work and so I tried to pause the program and use the memory window to set the register in memory. An interrupt is not generated however.

 

If you have any suggestions on how to cause an interrupt from the debugger I would be glad.

 

Regards,

 

Kilian

ラベル(1)
タグ(1)
0 件の賞賛
返信
1 解決策
1,904件の閲覧回数
kiliant3072
Contributor I

Answering my own question here I have to say it works now. Just writing to the appropriate GIC register does the trick.

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,905件の閲覧回数
kiliant3072
Contributor I

Answering my own question here I have to say it works now. Just writing to the appropriate GIC register does the trick.

0 件の賞賛
返信