Can i receive a demo project code of TCP communication betweene PC and MSC8156AMC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i receive a demo project code of TCP communication betweene PC and MSC8156AMC?

1,773 Views
jung-ilcho
Contributor I


Hi.

 

i'm testing about tcp communication between PC  and MSC8156AMC with uTCA RACK.

 

First, i try a demo program debugging of codewarrior. Demo name is "AMC_UEC0_net_demo" in codewarrior demos folder.

 

but it is not normally operating. MSC8156AMC did not send a packet after few minutes.

 

it seems like malfunction of QUICC Engine of msc8156.

 

so can i receive a demo program code of TCP communication betweene PC and MSC8156AMC?

 

thanks.

Labels (1)
0 Kudos
Reply
1 Reply

1,391 Views
lunminliang
NXP Employee
NXP Employee

Hello Jung-il Cho,

Some initial tips for this:

1. Check if UEC0 is enabled in the demo's configuration header file.

2. Check if DSP has correct RCW for UEC0.

3. Check if switch on the board is set correctly

4. Check if you connect on the correct RJ45

Regards

Lunmin

0 Kudos
Reply