An Error of booting up to DSP

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

An Error of booting up to DSP

2,551件の閲覧回数
hoaho
Contributor I

Dear all,

I am trying to boot an file named PHY.bin into the B4860 board. But the console window displays as:

==============================================================================

root@b4860qds:~# cd /ipc

root@b4860qds:/ipc#

root@b4860qds:/ipc#

root@b4860qds:/ipc# ./dsp_bt -h 1 -c 0 -i Debug.bin

===B4860QDS DSP boot Application (3.0.0) ===

SYSTEM MAP

DSP PrivArea: Addr=80000000 Size=7ff00000

Shared CtrlArea: Addr=fff00000 Size=100000

DSP Core0 M2: Addr=0 Size=0

DSP Core1 M2: Addr=0 Size=0

DSP M3: Addr=c40000000 Size=8000

PA CCSRBAR: Addr =ffe000000 Size=1000000

DSP CCSRBAR: Addr =ffe000000 Size=1000000

PA Shared Area: Addr=60000000 Size=f000000

DSP Shared Area: Addr=6f000000 Size=1000000

Loading Dsp image Debug.bin

 

 

Copy Part 80000000 1830

 

 

Copy Part 80002000 3008

 

 

Copy Part 80006000 2400

 

 

Copy Part 80009000 1eaa0

 

 

Copy Part f7f00000 607c

 

 

Copy Part f7f08000 1000

 

 

Copy Part f7f09000 1000

 

 

Copy Part f7f0a000 1000

 

 

Copy Part f7f0b000 1000

 

 

Copy Part c40000000 1000

 

 

Copy Part c40001000 1000

 

 

Copy Part c40002000 1000

 

 

Copy Part c40003000 1000

intvec_addr =8001a000 in L1 Binary

Before StarCore release ========

LCC_BSTRH=0x0

LCC_BSTRL=0x7ffff000

LCC_BSTAR=0x8110000b

GCR_CDCER0=0x0

GCR_CHMER0=0x0

DCFG_BRR=0xf

After StarCore release ========

LCC_BSTRH=0x0

LCC_BSTRL=0x8001a000

LCC_BSTAR=0x8100000c

GCR_CDCER0=0x3f0

GCR_CHMER0=0x3f00

DCFG_BRR=0x1f

BSTRL,BSTAR,CDCERO,CHMERO n DCFG_BRR set now

sleep 1, waiting for hw sem

sleep 1, waiting for hw sem

sleep 1, waiting for hw sem

sleep 1, waiting for hw sem

sleep 1, waiting for hw sem

sleep 1, waiting for hw sem

sleep 1, waiting for hw sem

sleep 1, waiting for hw sem

sleep 1, waiting for hw sem

 

===============================================================================================

are there anyone who know about the error HW SEM ?... Please give me a way to solve the problem!

Many thanks for your support!

ラベル(1)
0 件の賞賛
返信
2 返答(返信)

1,921件の閲覧回数
lunminliang
NXP Employee
NXP Employee

Hello Hoa Ho,

It may be waiting for other DSP cores to go up.

If this is multicore project, please change in os_config.h:

#define DP_SINGLE_CORE                     ON

#define  OS_MAX_NUM_OF_CORES      1

Have a great day,
Lunmin

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信

1,921件の閲覧回数
nikunjtapodhan
Contributor I

Hi Lunmin,

I also faced similar issue, I resolved it by doing following:

Just comment the function call   "osWaitForAllCores " getting called in b4860HetBootInitialize(), and you should be good to go for loading single core binary.

b4860HetBootInitialize-> Reference:

..\StarCore_Support\SmartDSP\source\arch\starcore\b4860_family/b486x.c

However I do get following issues in loading multicore image

1) When I load multicore dsp image :

(SIX CORES Configured and OS_Mulitcore=1, and also the OSwaitforallcores function disabled in het boot function)
1) dsp_bt -h 1 -c 0 -i c0.bin -c 1 -i c1.bin... -c 5 -i c5.bin -s shared.bin

but it still shows the same problem "waiting for hw  semaphore".

Any ways how to solve this problem for multicore??

2) I could run IPC integration example in smart dsp demo directory through power pc ,(IT IS A SINGLE CORE EXAMPLE)

I tried to convert it into multicore by making changes in os_config.h :

i) #define OS_NUM_OF_CORES                     OS_SOC_MAX_NUM_OF_CORES (i.e "6")

ii) OS_Mulitcore=1,

and also the OSwaitforallcores function disabled in het boot function.

Now the problem is the binaries getting generated are of unequal sizes:

core0.bin ->   200 kb

core1.bin->   15 kb

core2.bin->   15 kb

core3.bin->   15 kb

core4.bin->   15 kb

core5.bin->   15 kb

When i try to load this images , I get the same problem "waiting for hw  semaphore".

Binaries were generated using:

b4860_bin_creator.exe -cw '${SC_TOOLS_HOME}' -dir '${CW_Project}/ipc_integration_demo' -arch b4860 separate_shared_bin_files On

Any answers to this questions ??

regards

nikunj

0 件の賞賛
返信