Can i receive a demo project code of TCP communication betweene PC and MSC8156AMC?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Can i receive a demo project code of TCP communication betweene PC and MSC8156AMC?

1,778 次查看
jung-ilcho
Contributor I


Hi.

 

i'm testing about tcp communication between PC  and MSC8156AMC with uTCA RACK.

 

First, i try a demo program debugging of codewarrior. Demo name is "AMC_UEC0_net_demo" in codewarrior demos folder.

 

but it is not normally operating. MSC8156AMC did not send a packet after few minutes.

 

it seems like malfunction of QUICC Engine of msc8156.

 

so can i receive a demo program code of TCP communication betweene PC and MSC8156AMC?

 

thanks.

标签 (1)
0 项奖励
回复
1 回复

1,396 次查看
lunminliang
NXP Employee
NXP Employee

Hello Jung-il Cho,

Some initial tips for this:

1. Check if UEC0 is enabled in the demo's configuration header file.

2. Check if DSP has correct RCW for UEC0.

3. Check if switch on the board is set correctly

4. Check if you connect on the correct RJ45

Regards

Lunmin

0 项奖励
回复